AXIS#.SETUPREQBITS
Description
AXIS#.SETUPREQBITS is a bit-field that returns the set of parameters that needs to be set up before the drive can be enabled. The drive can only be enabled when this parameter returns 0.
-
-
If AXIS#.MOTOR.AUTOSET is set to 1 (parameters automatically calculated from motor ID data), then all values in the list will be initialized from the feedback device. Otherwise, the parameters must be set manually.
The following table lists the parameters which require setup for each motor type.
| Index | Bit | Default Value | Induction Motor V/f Open Loop (MOTOR.TYPE 2) | Induction Motor Closed Loop (MOTOR.TYPE 4) ) | Interior Permanent Magnet (MOTOR.TYPE 6) | Sensorless Permanent Magnet (MOTOR.TYPE 10) |
|---|---|---|---|---|---|---|
| AXIS#.MOTOR.IPEAK | 0 | 2 Arms | √ | √ | √ | √ |
| AXIS#.MOTOR.ICONT | 1 | 1 Arms | √ | √ | √ | √ |
| AXIS#.MOTOR.POLES | 3 | 6 | √ | √ | √ | √ |
| AXIS#.MOTOR.LDLL | 6 | 4 mH | - | √ | √ | √ |
| AXIS#.MOTOR.LQLL | 7 | 4 mH | - | √ | √ | √ |
| AXIS#.MOTOR.KE | 8 | 20 | - | - | √ | - |
| AXIS#.MOTOR.IMTR | 9 | 100 ms | - | √ | - | - |
| AXIS#.MOTOR.IMID | 10 | 0 Arms | - | √ | - | - |
| AXIS#.MOTOR.VOLTRATED | 11 | 230 Vrms | √ | - | - | - |
| AXIS#.MOTOR.VRATED | 12 | 1200 RPM | √ | - | - | - |
| AXIS#.MOTOR.LISAT | 13 | 1000 x AXIS#.IPEAK | - | - | √ | - |
| AXIS#.MOTOR.PHSADVK1 | 14 | 0 | - | - | √ | - |
| AXIS#.MOTOR.PHSADVK2 | 15 | 0 | - | - | √ | - |
| AXIS#.MOTOR.IDMAX | 16 | 1 Arms | - | - | √ | - |
| AXIS#.MOTOR.PITCH | 17 | 32 mm | - | - | - | - |
| AXIS#.MOTOR.VOLTMAX | 18 | 480 Vrms | - | - | √ | - |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer (bit-field) |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5017 |
1 |
5017 (0x1399) |
AXIS1.SETUPREQBITS |
Unsigned32 |
Read Only |
Yes |
|
70553 |
2 |
5017 (0x1399) |
AXIS2.SETUPREQBITS |
Unsigned32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.SETUPREQBITS |
5017 |
Unsigned32 |
Read Only |
- |
Related Topics